8/3/2010 12:59 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello RossF, Please find the attached file which gives you an idea aboutthe overview of simodrive converter system & how control card of the system can be configuered. Basically 611 drive system is designed for FK6, FT6& PH7 series motors with 1 VPPencoder systems. I don't think with FT5 series AC feed motors, with tacho & shaft encoder, (can you providethe details of of encoder of the motor) system will have optimised performance. However pls see this link which shall give you the detail information about Simodrive. http://www.automation.siemens.com/doconweb/content.asp?item=12410&cd=sinumerik_simodrive_04_2010_e&scope=all Hope this will help you. DEEP. AttachmentSIMODRIVE 611 U.pdf (337 Downloads) |
8/5/2010 4:40 AM | |
Posts: 2964 Rating: (478) |
Hello Ross.... Yes Simodrive 611 can control the servos if thepower module and themotor selection are done on 611A control card by switch settings which is available properly..... I am attaching the commissiong steps in the PDF which are easy to understand.... In your case note down the power module rating and motor type and the informations make the swtich settings on your 611A control card as given in the PDF,,,, you can also see the further information in DOCON web link attached for the further reference.... http://www.automation.siemens.com/doconweb/content.asp?item=12807&cd=sinumerik_simodrive_04_2010_e&scope=all Check it out.... Best Regards, Ekalavya Attachment611A startup.pdf (380 Downloads) |
Follow us on