10/5/2022 3:54 PM | |
Joined: 3/23/2022 Last visit: 3/10/2023 Posts: 1 Rating: (0) |
Hello everyone, I have a problem in a machine that runs a servo motor to turn a table around which is controlled by Simotion but suddenly it doesn't send output anymore even when it receieves the input from a beckhoff plc ,so i checked if the program still exists in the driver but i couldn't find it so i want to know if the someone deliberetly resetted the simotion or the flash card : 6AU1400-1PA23-0AA0 did get degraded over the years ? what is the average life time of such a flash card ? Thank you and i really appreciete your help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/06/2022 07:13:12New subject after splitting |
|
Follow us on