Industry Online Support
Technical Forum
9/16/2013 2:39 PM | |
Posts: 767 Rating:
|
Hello amsd, Your question is not an easy question to answer in a few sentences. It largely depends upon the application requirements for moving load plus the mechanics between the load and motor. Following is a link to SIZER for Siemens drives as a download location. This tool can be used to model the mechanics, determine the torques and speeds needed from the motor to move load per requirements of application, and the amount of current needed from the output of the servo drive. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objid=10804987&nodeid0=10804987&DataKey=10804987&treeLang=en&lang=en&extranet=standard&viewreg=WW&u=NDAwMDAxNwAA&siteID=cseus Best Regards, Deputy |
Follow us on