1/19/2015 6:35 PM | |
Joined: 12/18/2014 Last visit: 5/25/2024 Posts: 33106 Rating: (4087) |
In configuration mode, only the parameters can be changed if the 0BA8 is in operator mode, no admin mode. To enter the configuration mode, press the ESC button for 2 seconds to be longer. Then, the cursor jumps to the field whose value can be changed. Accept with OK. There you can use the cursor keys left / right in the Select the appropriate number, change the value using the cursor up / down. Is set to the desired value, again accept with OK. In the simulation, you do it with a double-click on the field (see attachment). Do want an example (for 0BA8 or other)? AttachmentTimer setting over display or TDE.zip (208 Downloads) |
This contribution was helpful to1 thankful Users |
1/19/2015 6:46 PM | |
Posts: 15 Rating: (0) |
Perfect ! that's all i needed to know ; Thanx allot ! |
This contribution was helpful to1 thankful Users |
1/19/2015 6:50 PM | |
Joined: 12/18/2014 Last visit: 5/25/2024 Posts: 33106 Rating: (4087) |
You're welcome! |
1/20/2015 11:36 AM | |
Joined: 12/18/2014 Last visit: 5/25/2024 Posts: 33106 Rating: (4087) |
Wrong idea. |
Last edited by: ixo65 at: 1/20/2015 12:02 PM |
|
1/20/2015 12:05 PM | |
Posts: 15 Rating: (0) |
Other solutions ? |
1/20/2015 12:05 PM | |
Joined: 12/18/2014 Last visit: 5/25/2024 Posts: 33106 Rating: (4087) |
With LOGO! how can you store analog values as non-volatile? http://support.automation.siemens.com/WW/view/de/25174196 English link: http://support.automation.siemens.com/WW/view/en/25174196 |
Last edited by: Min_Moderator at: 1/20/2015 1:06 PMAdd English link |
|
1/23/2015 2:30 PM | |
Posts: 15 Rating: (0) |
Thank you, I've been trying to figure out how this schematic works, but i'm still struggling with it.
|
Follow us on