3/4/2021 3:49 AM | |
Joined: 8/11/2017 Last visit: 3/15/2023 Posts: 7 Rating:
|
Is there any information on setting up the slots in transfer areas? I tried setting it up the way it is in step 7 starting at slot 4, but recieved errors on compile. I then started my telegrams at the first slot and compiled with no error but no communication when hardware configuration is loaded. This was an attempted migration from step 7 into tia 15.1. Also the free telegrams were already predefined and I didn't want to change all that code, so I used universal modules with axis disconnects between each axis. Firmware versions matched, so I am not sure what the issue was. ------------------------------------------------------------------------------------------ |
Last edited by: Ztay8514 at: 03/04/2021 03:51:03Last edited by: Jen_Moderator at: 03/04/2021 10:32:17New subject after splitting |
|
3/4/2021 6:32 AM | |
Joined: 5/12/2006 Last visit: 3/30/2023 Posts: 21352 Rating:
|
screens of the configuration need |
3/4/2021 3:02 PM | |
Joined: 8/11/2017 Last visit: 3/15/2023 Posts: 7 Rating:
|
Screenshot of hardware config |
3/4/2021 4:48 PM | |
Joined: 7/7/2010 Last visit: 3/29/2023 Posts: 13213 Rating:
|
Do you have a screenshot of the step7 hardware configuration for the same module? Does it have 17 slots filled with things? You do not require the slot fillers for slots without I/O telegram data. Just delete those since are (typically) not required.
|
science guy |
|
Follow us on