9/20/2016 2:04 PM | |
Joined: 8/4/2014 Last visit: 10/31/2024 Posts: 3 Rating: (0) |
Can someone please assist me... how do i setup my Mobi pannel 277 with my scalance 788-1 rj45. Oo and i have 1511-1PN CPU ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/21/2016 10:11:04 AMNew subject after splitting |
|
9/21/2016 8:28 AM | |
Joined: 8/3/2009 Last visit: 11/18/2024 Posts: 14181 Rating: (1774)
|
Hello Dee707 First of all the Mobiel Panel acts like a normal Ethernet Panel so to configure the Communication use the following FAQ: https://support.industry.siemens.com/cs/de/en/view/89852595 The other Thing is to configure the WLAN communication, so the physical connection. And this is not very different to an access Point you use at home. Create a WLAN with a SSID and Authentication in the SCALANCE. Then configure the WLAN Settings at the Panel and then the connection should work. If the CON LED is on continously then the WLAN connection is OK. Do a Ping and then you could transfer the Project. If you had a F Panel/CPU then it is much more tricky. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on