2/1/2012 8:09 AM | |
Posts: 140 Rating: (0) |
Hello Experts. I am facing an issue that MY PLC’s (315T-2DP CPU) SF LED is continuously blinking and I can’t even establish a connection with my PLC to download any program into it. I have attached the project that I am using. Please suggest the solution asap. Is it a hardware problem? It was working fine until I reset it using the attached procedure. Thanks! Attachments7300 cpu 31xc and cpu 31x operating instructions en US en US 1 pdf.pdf (598 Downloads) |
2/2/2012 7:06 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
Hello, What about MMC? Does only SF blinks there? Best regards, Hristo Mihalev |
2/2/2012 8:18 AM | |
Posts: 140 Rating: (0) |
Yes for MMC also,only SF LED blinks same way :( |
Last edited by: Khyzer at: 2/2/2012 8:27 AM |
|
2/2/2012 8:26 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
Do yo have another MMC in order to test it? Meanwhile I suggest you Support Request... Best regards, Hristo MIhalev |
2/2/2012 8:29 AM | |
Posts: 140 Rating: (0) |
No I don't have extra MMC at the moment. Can you list out possible causes of this issue? Thanks!
|
2/2/2012 9:28 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi Can you remove the MMC card and check. Have fun.... |
Jazz |
|
2/2/2012 9:40 AM | |
Posts: 140 Rating: (0) |
Yes I have removed the MMC and SF LED still continue to flash! |
Follow us on