10/7/2015 7:34 PM | |
Joined: 3/30/2011 Last visit: 10/9/2024 Posts: 736 Rating: (256) |
Hello, Wath is the program you reinstall?? To see PLC diagnostic buffer you need Step7 v5.4 software and MPI-PROFIBUS interface. Do you have this? In this manual (cap 10.8) some indication about leds meaning. Regards |
★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
10/8/2015 9:46 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi, what SW do you have to load your program in the 314C? Did you load the HW-Config with other connection parameters? When the SF-LED is on, you have to look online. Further diagnostic is available there. If you can´t go online try to reset the CPU to delivery state. See the following manual on page 197 how to do it. SIMATIC S7-300 CPU 31xC and CPU 31x: Installationhope this helps, regards, |
FCK WAR! |
|
Follow us on