9/3/2014 11:01 PM | |
Posts: 3 Rating:
|
Hello, I need to read data from a MTS Temposonic sensor with Profibus interface. I've already import the GSD file from MTS and add the device in my project (TIA V13). If I understand the SFB 52 function, I've to use the folowing parameters : ID = 278 INDEX = 68 MLEN = 1 Byte (See in MTS datasheet) RECORD = MTS_STATUS (Data type = Byte) on MTS_DB database This configuration didn't works, the var MTS_STATUS didn't change. Does someone have advice to fix my problem? I've attached snapshot of my project. Thanks
AttachmentSFB 52.zip (368 Downloads) |
9/3/2014 11:28 PM | |
Posts: 3 Rating:
|
The sensor is available in the tree but I don't know how to do the "profibus cyclic communications", do you have documentation or a bloc to use? Thanks
|
Follow us on