3/5/2018 11:02 AM | |
Joined: 3/14/2008 Last visit: 6/6/2024 Posts: 2070 Rating: (928)
|
Hi Ahmed.tn, I assume you are talking about a SFC instance (A SFC inserted in a CFC chart). In this case, the SFC instance is based on a SFC type which can found in the master library or project under Component View. The error means that you have changed the SFC type and thus the SFC instance, but it is not updated in your project (where you want to copy the CFC with SFC to). You have to update the SFC type in your project as well. This can be done by simply copying the SFC type to your project or update the SFC type via Component View->Charts->Update Block Types from your master library. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
3/5/2018 1:01 PM | |
Joined: 3/14/2008 Last visit: 6/6/2024 Posts: 2070 Rating: (928)
|
Hi, Can you show me a screenshot of the CFC you try to copy and the error it gives? The CFC from where do you copy this? Is this an old backup or different multiproject? Can you give me some more information to determine the root cause? |
If I could help you, you can use the RATE button. Thank you. |
|
3/5/2018 1:59 PM | |
Joined: 9/9/2015 Last visit: 6/7/2024 Posts: 727 Rating: (270) |
If possible,please make sure your cfc version is updated to the latest one. Siemens have bug fix on the sfc related issues in the previous version. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
3/5/2018 2:07 PM | |
Joined: 11/10/2010 Last visit: 6/5/2024 Posts: 165 Rating: (8) |
tyanks Jazztai for answer, can you tell me please how to update the SFC In the MP .?? |
3/12/2018 1:53 PM | |
Joined: 11/10/2010 Last visit: 6/5/2024 Posts: 165 Rating: (8) |
Hello, thanks for your answer, i tried as you proposed, but always the same error message |
Follow us on