12/9/2021 8:23 AM | |
Joined: 4/26/2011 Last visit: 12/22/2023 Posts: 25 Rating: (0) |
Dear All, I am Creating SFC Type with by following "Process Control System PCS 7 Getting Started Part 2 (V7.1) 03/2009 A5E02122247-01 page-135" Training. In Characteristics when I am entering Values of "Block Contacts" in Block Column I cannot able to find "CTRL_PID" Block in Drop Down List. I can only see "Valve" and "Motor" Block. I cannot select "CTRL_PID" Block, my task is stuck and stop. would anyone can share how it can be solved. see attached file with images. Thanks & Regards AttachmentProcess Control System PCS 7 Getting Started Part 2 SFC type issue.docx (303 Downloads) |
12/10/2021 9:14 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, It means the block does not exist in your project/library (don't know where you placed the SFC type). Add the block to the library and it can be found. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on