8/24/2019 2:44 PM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating:
|
Hello Moderator, When i was using SFCtype in PCS7 9.0, i faced an issue. Unfortunately i copied some text from the "Name" field of process values available under characteristics, pasted those content on I/O name field, My SFCType editor got completely closed certainly. It wasn't showing any error, I got confused and later found that the length of the textual content crossed the limit (24 character), (Attached image-"SFCType_IOname_Issue") Also, the SFC was not closed properly, It was showing "Chart is being edited" pop-up during on next access, (Attached image-"SFCType_IOname_Issue2") Then, I Reopened the SFCType, Filled the I/O name by typing on the field, It wasn't creating such errors even after typing the character input more then 24. It would be better if it shows an error or warning message instead closing the complete SFCType, Users may get confused in handling it, Already some other functions of PCS7 having the warning and help details for the same type of issues (Attached image-"Warningonotherevents" AttachmentSFCType_IOname_Issue.zip (30 Downloads) |
Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
8/28/2019 11:24 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hello Maruthakasi_S, thank you for sharing your information with us. The handling with too long names by the SFC type is a bug. Can you report this via Support Request, so that Siemens can fix it in the next update. A little tip:
With regards |
This contribution was helpful to
1 thankful Users |
Follow us on