6/3/2022 8:12 PM | |
Joined: 2/3/2021 Last visit: 5/5/2023 Posts: 1 Rating:
|
Hi, This is a simple bit shift program library based on Array, that can shift a single bit. Also, you can give the boolean values "0" and "1" from a DI or Memory. You can also use this for shifting integer values. Just change the data type of the array on the function DB. similarly, you can also change the length of the array if needed. A sample program is also attached along with it. AttachmentBIT Shift Lib.zip (220 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on