10/10/2022 1:29 AM | |
Joined: 6/19/2018 Last visit: 8/21/2024 Posts: 158 Rating: (0) |
Hi, I have a Step7 v5.5 Let me know Shortcut keys for "Modify address to 1" Best regards, Lee |
10/10/2022 5:44 AM | |
Joined: 1/21/2013 Last visit: 11/11/2024 Posts: 3256 Rating: (507) |
Hi Lee, SIMATIC STEP 7 has different editors with different behavior. So it depends on the editor. At the "Variable Table" editor, you can use Ctrl + 1 to modify a value to 1 (and Ctrl + 0 to modify to zero). In the LAD/STL/FBD editor, there is no shortcut to modify the value. But you can use "Control at Contact" to easily modify the value using the mouse. For details, please refer to chapter 26.6 of the programming manual 'Programming with STEP 7'. Kind regards |
Follow us on