1/3/2018 2:35 AM | |
Posts: 3 Rating:
|
Good day Sir, With regards to my problem in communication between my CLV630-6120 Barcode Scanner and a S7-1200 1215C DC/DC/DC. I took time in studying the parameters of my barcode scanner and I found out that it has a PROFINET IO On-Board. So, I replaced the setting to PROFINET IO instead of ETHERNET/IP. The connection type of the barcode scanner is Ethernet Cable so, I connect it on the Port 1 (X1P1R) of my PLC. Now, I checked the "Online Access" of the TIA Portal V13 and when I searched for devices, I'm surprised to see that the CLV630-6120 came out on the search list. it means that the PLC can already see the barcode scanner. Then, I started to download the GSDML File and the Function Block provided on sick.com then import it on the TIA Portal. Next, I connected the 2 devices on the "Device and Networks" of the TIA Portal and start to program the downloaded function block. One feature of the function block is to conduct a Software Trigger via Command (PLC will trigger the barcode to conduct scanning procedure) After that, I conduct a system testing/online testing and here is the result: - When I monitor the connection of the devices, it is on the Green Indicator (does it mean connected?) - I connected to I0.0 a photoelectric sensor to trigger the #Req parameter of the function block. When I triggered the sensor, the #ReqBusy turns ON and the barcode scanner didn't conduct a scanning and ends up in an Error stated (No action executed). Do I still have regarding communication of both devices? Please help me with this. Thanks! AttachmentSTATUS REPORT 1.02.2018.pptx (415 Downloads) |
12/4/2019 5:49 AM | |
Joined: 4/18/2014 Last visit: 7/4/2024 Posts: 253 Rating:
|
Please share the above Manual if any one have |
4/19/2024 8:35 AM | |
Joined: 4/19/2024 Last visit: 4/29/2024 Posts: 1 Rating:
|
good day , i have the same probleme , any advice |
Follow us on