11/27/2017 12:18 AM | |
Posts: 1 Rating: (0) |
First of all, receive a cordial greeting for all the members of this group. I write to you because I have a great challenge to start a numeric lathe which is not operational since 2013. This work for a short period of 3 months after its installation. I present the alarms on the HMI since then it says, 120202 "WAIT CONNECTION WITH CN / PLC" Through the X127 port I could connect with laptop and with the WinSCP program with the IP address 192.215.1, user: manufact and password: SUNRISE, get access to the compact flash memory and make a small backup of what is found. In spite of that, according to the manual SINUMERIK 840D sl BASIC SOFTWARE AND SOFTWARE OF HANDLING. START UP MANUAL. I have managed to make a series of solutions that they suggest, but without being able to make any effect. I come to you to see what recommendations they give me to be able to solve the problem with numerical lathe. Greetings. Alberto Torres. [snip] ------------------------------------------------------------------------------------------ Attachmentcompressjpeg.zip (105 Downloads) |
Last edited by: Jen_Moderator at: 11/27/2017 1:26:31 PMRemoved personal contact data. Last edited by: Jen_Moderator at: 11/27/2017 1:36:42 PMNew subject after splitting |
|
2/24/2018 11:40 PM | |
Posts: 4 Rating: (0) |
you fix it ? if not i will help you .... |
Follow us on