3/24/2009 8:20 AM | |
Posts: 100 Rating:
|
Hi to all I attached the another configuration below.Is it possible to establish the GPRS communication with GPRS modem less than3. |
3/24/2009 2:30 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello Maybe is better to ask in AB forum or AB Hotline center is this possible and how to establishe connection with this hardware. If we talk only for siemens hardware, it doesn't problem to prepare this connection. Look at following link: How do you configure a VPN tunnel between a PC station with Windows XP SP2 and SCALANCE S61x V2.1 via the Internet with the Microsoft Management Console? Basicly idea is to use CP in Siemens PLC and AB PLC to connect in one ethernet network, and after using scalance to connect with remote PC. Hope this will helps. best regards |
Follow us on