2/26/2016 3:03 PM | |
Posts: 31 Rating: (0) |
good evening, can anyone tell me how to download and upload program in elfa drives. |
2/26/2016 4:05 PM | |
Joined: 9/27/2006 Last visit: 5/14/2024 Posts: 12257 Rating: (2668) |
Hello ganivz; ELFA drives are made by Siemens, but they belong to a division we have little access to, Electromobility. http://w3.siemens.com/topics/global/en/electromobility/pages/powertrain-commercial-vehicles.aspx They seem to have no extranet access or support site (such as IA&D has, with this forum). From the Siemens Global site, this is the only link I found to Electromobility.. ELFA drives and component s are designed for electric and hybrid vehicles, and I am not sure if a user is allowed to download a program to the controllers. See for example this article (from 2004) on the marketing of the ELFA Thundervolt drive: http://www.altenergymag.com/content.php?issue_number=04.04.01&article=thundervolt 2.4. Vehicle Control and Diagnostics
ISE has developed a proprietary system control architecture for use with the ThunderVolt™-ELFA™ drive system. The hybrid and drive control software is an integral part of the system. The vehicle interface is provided by the vehicle controller, which is based on a high speed automotive J1939 multiplexing system manufactured by STW in Germany. It also provides an interface to displays and standard vehicle electronics such as GPS. The CAN bus architecture of the ThunderVolt™-ELFA™ vehicle control system has been greatly simplified over the last three years. All major vehicle subsystems (Motive Drive, APU, Energy Storage, Vehicle Control, and Accessories) communicate on one single CAN network. This simplifies and improves vehicle data acquisition and maintenance. All major vehicle subsystems can be accessed via one data port. Custom programming is performed jointly by ISE and Siemens. The computerized control network on the bus relies on distribution boxes to monitor, fuse, supply, and/or switch power to high power components. The only thing I can suggest at this time is to use the contacts link provided by the Siemens Global site and ask the Electromobility techs your questions directly: mailto:LDTDHDSWebmaster.industry@internal.siemens.com Hope this helps, Daniel Chartier
|
This contribution was helpful to1 thankful Users |
2/28/2016 9:43 AM | |
Posts: 31 Rating: (0) |
thank you for your response, daniel chartier |
Follow us on