3/29/2012 3:06 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating:
|
Hello Siemens EPLAN Macros are now available in EDZ format. The FAQs following FAQs have been provided to guide users for importing macros in EPLAN format. http://support.automation.siemens.com/WW/view/en/48074331 http://support.automation.siemens.com/WW/view/en/57420555 The problem is,however this tool has to be downloaded from EPLAN portal. Although the tool is supposed to be free for all Genuine EPLAN users, it cannot be downloaded unless you subscribe to annual software update contracts from EPLAN ( for which they charge huge amounts ). Therefore a large no of EPLAN users are not able to use the EDZ files. It is suggested that the should be an option in CAx Shopping Cartfor downloading Macros in Windows Macroformat ( Aswas available earlier ). Thanks Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
5 thankful Users |
10/24/2013 11:02 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating:
|
Hi Ritvars Rižikovs This is a wonderful tip Thanks a Ton Cheers Navnag |
There is no such thing as the last bug in a program |
|
8/14/2014 6:52 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating:
|
Hello Ritvars Rižikovs Some of the new Macros ( e.g. SINAMICS / SIMOTION ) , I am not able to edit the preset Texts inside the macro. Also some of the texts are at an angle, besides there is a large text " {{SIEMENS}} " which looks horrible ... I Do not know how to adjust is Font and Angle I am attaching one such Macro as an Example. Pl help Thanks Navnag
AttachmentEPLAN_Macro_Sample.pdf (5161 Downloads) |
There is no such thing as the last bug in a program |
|
5/23/2016 10:51 PM | |
Joined: 1/14/2016 Last visit: 3/23/2023 Posts: 29 Rating:
|
Good evening, What about 3D mounting layout for the Pro Panel version? Are there any downloads for this version? |
Follow us on