2/11/2016 6:12 PM | |
Joined: 9/27/2006 Last visit: 7/17/2024 Posts: 12268 Rating:
|
Hello dcclark; In the Technical Data section of the Appendix of following manual you can find this table of protocol drivers and PLCs (see attachment). SIMATIC HMI HMI devices Comfort Panels https://support.industry.siemens.com/cs/ww/en/view/49313233 It simply states that any Allen-Bradley (Rockwell) PLC communicating over Ethernet/IP can be connected to a Comfort Panel. Unless there is a non-standard implementation of Ethernet/IP in the MicroLogix 850 you should have no particular problem exchanging data between the Rockwell PLC and your TP 1500. I have worked with Rockwell PLCs programmed with Logix 5000 software and had no problems connecting these with Siemens panels using Ethernet/IP. I have not worked with the new Connected Component Workbench software yet; but Ethernet/IP standards are usually maintained throughout a product range, so I do not feel there should be issues. In any case, come back to us if there is a fault detected. Hope this helps, Daniel Chartier |
This contribution was helpful to
2 thankful Users |
Follow us on