6/10/2019 8:47 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Stuxnet90, Entry should be in STEP 7 Additional Software conference. For F datatypes, u should use CFC. For standard data types, STL/LAD etc. is permitted. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
This contribution was helpful to1 thankful Users |
6/10/2019 9:18 AM | |
Posts: 2 Rating: (0) |
Hello Sachinpatke, //Entry should be inSTEP 7 Additional Softwareconference.// sorry i didn't knew that. how can i move this to that page? //For F datatypes, u should use CFC. For standard data types, STL/LAD etc. is permitted.// So my assumption is correct, we only need CFC to convert F data type to normal data type. |
6/12/2019 1:21 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Stuxnet90, F_LAD or F-FB are used in distributed safety. It is used in machine or automotive automation. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on