Industry Online Support
Technical Forum
11/26/2009 1:34 PM | |
Joined: 8/25/2007 Last visit: 6/4/2022 Posts: 13 Rating: (0) |
I am having a problem with a Simatic Batch recipe transition which uses a process value as an operand as part of it's condition. Its the 1st time I've used a transition that looks at a process value and have followed the instructions in the Simatic Batch Manual (Creating and inserting user process tag types in CFC charts). When the recipe tries to evaluate the state of the process value, a '?' is seen in the online properties of the transition. See attached file for screenshots of online status and configuration. Any help or comments on the use of process variables would be greatly appreciated thanks Attachmentprocess variable batch problem.zip (76 Downloads) |