1/10/2018 9:34 AM | |
Joined: 11/19/2015 Last visit: 11/29/2023 Posts: 8 Rating: (1) |
I'm using SIMATIC IOT2000 I/O Shield on IOT2040. 1. Am I right that if i want in linux shell set the pin to high, I just overwrite /sys/class/gpioXXX/value to "1"? 2. Acording to IO-Operating instruction PDF the DQ1 is mapped to D7.Where is the table, at https://communities.intel.com/thread/55920, showing me the suitable gpio port for linux shell? ------------------------------------------------------------------------------------------ |
Last edited by: kurtl at: 1/10/2018 9:42:32 AMLast edited by: The Helping Hand at: 1/10/2018 10:02:03 AMNew subject after splitting |
|
3/23/2018 7:31 AM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7957 Rating: (162) |
New question published by Quentin_soluTech is split to a separate thread with the subject SIMATIC IOT2000 I/O Shield on IOT2040 - Standard one only has an input frequency of 20Hz max but need higher frequency. . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on