3/7/2023 3:20 PM | |
Joined: 5/6/2022 Last visit: 10/18/2024 Posts: 470 Rating: (94) |
Hi AutoGen_5646659, I can think of the following possible reasons: - Have you run all installations as Administrator? Maybe you can, after installing the new version of Windows, reinstall the softwares as Admin again? - Maybe you have a firewall/antivirus activated that could be causing a blockage? - Have you checked the compatibility of the software with your OS? Because it seems to me that some of them are not compatible in this environment. I share with you the excel where you can check it since I don't know if you have updates, the build of your OS... Best regards! AttachmentMicrosoft-Windows-Server_en_2023-02-27 (2).xlsx (537 Downloads) |
If this Information really helps, you could use the Rate function |
|
Follow us on