3/31/2017 4:43 PM | |
Posts: 26 Rating: (1) |
i try to upload the program but it doesn't work 'invalid file" |
3/31/2017 4:54 PM | |
Posts: 26 Rating: (1) |
hi thats my program this plc program was connected with wincc hmi project i delete the hmi project because the file was with large size thnx alot AttachmentCOMP-SYS1.zip (248 Downloads) |
3/31/2017 5:35 PM | |
Joined: 4/11/2012 Last visit: 9/6/2024 Posts: 181 Rating: (34) |
To make it easier, what should be done to activate the outputs? |
3/31/2017 8:32 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33783 Rating: (4195) |
I have corrected your program all outputs are only assigned once.
AttachmentCOMP-SYS1_V2.zip (226 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on