9/12/2013 11:59 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (133) |
Hello, use the tape combination <Strg>+<Alt>+<Del> and select in the follow dialog "Start Task Manager". In register "Processes" you can see the processes which are running and using their working storages. You can here stop the processes of not important applications. Other reasons could be an incompatibility between STEP 7, Windows operating system and an optional software package. See also the informations of the FAQ: http://support.automation.siemens.com/WW/view/de/24059046 With best regards |