1/8/2020 1:54 PM | |
Joined: 2/16/2017 Last visit: 6/13/2024 Posts: 17 Rating: (1) |
Hi Schufri I am using a single PLC (Not even Redundent) for WinCC. |
1/8/2020 2:08 PM | |
Joined: 2/16/2017 Last visit: 6/13/2024 Posts: 17 Rating: (1) |
I have attached ALM pic as requested. i have Created one Named Connection and only one PLC(Not even Redundent). |
1/16/2020 8:16 PM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating: (24) |
Hai Arshad73, Sorry for the delayed replay, I looked into your picture. Now, there are a few pieces of information for you. Which type of network ethernet adapter are you using for communication? If its special adapter except for IG_General (Standard Ethernet interface) you need to go for SIMATIC NET IE SOFTNET-S7 LEAN license. If your communication card is a Standard Ethernet interface, you need to buy a Simatic BCE license. When you are configuring OS single station, you should have a BCE license. I couldn't see it on your ALM list. Also, Please verify your ALM & SIMATIC WinCC License service is running under the windows "service" list. Look at the attached image and get the manual from below link: |
Last edited by: Maruthakasi_S at: 01/16/2020 20:19:45Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
1/23/2020 8:38 PM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating: (24) |
Hai Arshad73 , You are welcome, You can rate the post whichever helps you. Basically the purpose of Simatic HARDNET IE S7 is different. It will be used for H systems configurations widely. Not in OS single station architecture. Whenever server network communication fails with one CPU over named connections, the WinCC database itself will switch over(Act of Simatic NET) the connection to another rack of PLC. So, this Redconnect license allows the WinCC database to do that job. Version related to the family of CP card used on server PC and Simatic NET version. Kindly check in the manual ... |
Last edited by: Maruthakasi_S at: 01/23/2020 20:56:08Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
Follow us on