2/20/2011 10:07 PM | |
Joined: 10/7/2005 Last visit: 7/30/2024 Posts: 3013 Rating:
|
Hello Luay Khoury it's hard to say what you need without more details about your requirements. My questionsare: 1.) Do you want to use ProTool (I wouldn't as it is "history") or WinCC or WinCC flexible? 2.) Are you fixed or flexible concerning usage of either PPI, MPI, Profibus or Ethernet? 3.) If its ProTool or WinCC flexible, will it be Panel based or PC based Runtime? Anyway, once you narrowed your choicesdown, you'll find plenty of manuals,FAQ's and forum posts at https://support.automation.siemens.comand below are a few pre-emptively selected ones: SIMATIC HMI WinCC flexible 2008 Communication Part 1 What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options? What are the options for accessing an S7-200 with WinCC? S7 200 - configuring PC communications FAQ's I hope this helps |
Cheers |
|
2/23/2011 5:25 AM | |
Joined: 10/7/2005 Last visit: 7/30/2024 Posts: 3013 Rating:
|
Hello Luay Khoury it seems you already managed to find the answers yourself based on the supplied links, for everyone else interested in in how this continues, please continue reading HERE. |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on