10/14/2009 2:30 PM | |
Joined: 4/24/2006 Last visit: 7/3/2024 Posts: 8708 Rating:
|
Dear FernandoCosta, Here is a link, about cables you can use to transfer project: http://support.automation.siemens.com/WW/view/en/19109408 For OP27 it is possible to use Serial cable (6XV1440-2KH..) or MPI/Profibus Here is a link, where you can find out Pin layout of serial cable (6XV1 440-2KH..) http://support.automation.siemens.com/WW/view/en/29034071 When you power off panel. Then push and hold the buttons ESC and UP. Power on panel. Then you can release the buttons. (It should go in download mode) Best regards, Wizard |
10/14/2009 2:53 PM | |
Joined: 4/24/2006 Last visit: 7/3/2024 Posts: 8708 Rating:
|
Hi, I guess you have seen Chapter 14.2 of manual: http://support.automation.siemens.com/WW/view/en/1142800 Mind that Transfer mode is Download mode. Best regards, Wizard |
10/14/2009 4:01 PM | |
Posts: 13 Rating:
|
appears SyncTel on OP27... and then Line Error 0... so pc reboots... |
10/14/2009 4:07 PM | |
Joined: 4/24/2006 Last visit: 7/3/2024 Posts: 8708 Rating:
|
Hi, You mentioned COM4. Does it mean you use an USB/RS232 convertor? That could be a problem. Best regards, Wizard |
10/14/2009 4:13 PM | |
Posts: 13 Rating:
|
Yes... I´m using one of them... My pc doesn´t have a serial port... so I need to use that... Can´t I use? |
10/14/2009 4:38 PM | |
Joined: 4/24/2006 Last visit: 7/3/2024 Posts: 8708 Rating:
|
Dear FernandoCosta, I'm afraid it is not possible to use USB/RS232 convertor. Have a look at this link: http://support.automation.siemens.com/WW/view/en/13904923 Best regards, Wizard |
Last edited by: Wizard at: 10/14/2009 4:39 PMOoops, looks like link is not working anymore. You should contact Siemens Representative. |
|
10/14/2009 4:44 PM | |
Posts: 13 Rating:
|
ok... thank you for helping! |
Last edited by: FernandoCosta at: 10/14/2009 4:49 PM |
|
Follow us on