10/16/2024 9:04 AM | |
Joined: 5/6/2022 Last visit: 3/26/2025 Posts: 578 Rating:
|
Hi AUNI_ROSHINI, This error can be due to many things, as I have seen it and it is often difficult to diagnose. However, to start with I would recommend you to check the following: - The items listed on page 9 - ""Partly running" status": "Readme WinCC Unified Runtime" Also check the attached file in case it could be due to some points specified. Finally, does this problem occur only with this project? Or with any other that you create new simple? Best regards!
Attachmentpartly running.pdf (98 Downloads) |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on