7/25/2021 9:01 AM | |
Joined: 3/30/2020 Last visit: 3/20/2023 Posts: 3267 Rating:
|
Hello. Consider the use of a signal board (SB). This is an add-on that clips into the front of the CPU. This is a better option than changing the CPU. Find out more by reading the S7-1200 System Manual [LINK]. Best health. EDIT: The pulse outputs that are mentioned is a software ability that can only be used when using a signal board. |
Last edited by: qwazee at: 07/25/2021 09:03:49Add in response to topic starter's comments Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
2 thankful Users |
7/25/2021 9:13 AM | |
Joined: 12/23/2020 Last visit: 5/9/2022 Posts: 16 Rating:
|
Thanks a lot |
Follow us on