10/7/2021 7:01 PM | |
Joined: 5/27/2021 Last visit: 8/1/2022 Posts: 257 Rating:
|
Hello SIOS Forum Community, if you have not yet had any contact with the SIMATIC S7-1200, then the Starter Kits are the ideal introduction. With the six available packages, different tasks can be realized flexibly and economically: From engineering with the TIA Portal, to the integration of HMI panels, to solutions for fail-safe applications. In addition, we offer you further tools and assistance for getting started. In each of the 6 Starter Kits is always included in addition to the CPU 1212C: - Input simulator - a cable IE TP Cord 2 meters (to connect the programming device with the S7-1200) - Software SIMATIC Step 7 Basic in the TIA Portal Until further notice one SIMATIC OPC UA S7-1200 Basic license each will be enclosed additionally! The Starter Kits are delivered in the smart TANOS - Systainer - transport box. Another tip: All starter kits are only available in the AC/DC/RLY variant. Further information about the starter kits: SIMATIC S7-1200 Starter Kits with STEP 7 Basic V16 Note The procedure described in this article refers to the time of writing this article (status: May 2021). With kind regards SIMATIC International Technical Support Hub |
Follow us on