8/12/2015 4:47 PM | |
Posts: 74 Rating:
|
Dear all, I have one basic question about CPU. In attachment I will post picture, Is this X presenting number 2? Does it matter which number is written in that corner? And if it does.. is it about the speed of the CPU? Or for example if I have CPU with number 1 in corner, are my possibilities limited so I can't use some OB's, SFC's etc. which are allowed to CPU with that number 9? Or am I wrong? If someone can explain me what that number in corner means I would be very grateful.. Im talking about same CPU with 2 different numbers.. With best regards, Marko |
8/12/2015 4:55 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello Markozg, The X is the hardware version (E-stand) have a look: Is for panel but is the same: How can you determine the "E-Stand" (hardware release) of an operator panel? |
This contribution was helpful to
2 thankful Users |
8/12/2015 5:03 PM | |
Posts: 74 Rating:
|
Dear Ste39, Thank you for your feedback, Can you explain me diference between hardware E-Stand 01, and 09 ? Thank you so much With best regards, marko |
8/12/2015 5:06 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Dear marko, In "poor word" the 01 is the first version and the 09 is the most recent you can say "improvements Hardware" |
Last edited by: Ste39 at: 8/12/2015 5:07:54 PM |
|
This contribution was helpful to
1 thankful Users |
8/12/2015 5:21 PM | |
Joined: 5/12/2006 Last visit: 4/4/2025 Posts: 22607 Rating:
|
Hi,
or improvements Software The E-Stand is also incremented with a new FW Version
Christoph |
This contribution was helpful to
1 thankful Users |
8/12/2015 10:24 PM | |
Posts: 74 Rating:
|
Hi guys, By purchasing the better hardware for example E-Stand 09, which is the main difference comparing to E-Stand 01 ? Can someone which are the advantages of the newer version E-Stand 09... If you know some details.. Thank you so much, Best regards, Marko |
Last edited by: markozg at: 8/12/2015 10:25:13 PM |
|
8/12/2015 11:18 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Dear Marko, As an example a Input card with E-Stand 01 , maybe if there is a defect, Siemens improving it and goes to an E-Stand 02 this is for CPU with improving Hardware and Firmware also as said our friend Christoph |
Last edited by: Ste39 at: 8/12/2015 11:19:48 PM |
|
This contribution was helpful to
1 thankful Users |
8/13/2015 9:24 AM | |
Posts: 74 Rating:
|
Dear all, Just one question.. By improving SW and FW am I able to use some new blocks which were unavaible in previous version? New blocks like some new OB's, SFC's etc..... That are some general improvements made by Siemens, but I can't find on Internet which the improvements were made.. Im interested in this, please help Thank you in advance, With best regards, Marko |
Last edited by: markozg at: 8/13/2015 9:33:29 AM |
|
8/13/2015 9:45 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello Marko, More than CPUs are improved and more have development opportunities. Give us a code like CPU 6ES7 31x-xxxxx-xxxx |
8/13/2015 9:47 AM | |
Joined: 5/12/2006 Last visit: 4/4/2025 Posts: 22607 Rating:
|
Hello,
you can look in the delivery notes of the FW Versions if new blocks are released with the FW, normaly no change on the SFC is made.
OB, FB, FC ist usercode and not from siemens! Hw changes not documented for users! Regards Christoph |
This contribution was helpful to
2 thankful Users |
We are working on a new user interface with better overview and more relevance.
Follow us on