12/9/2014 12:44 PM | |
Joined: 5/12/2006 Last visit: 7/31/2024 Posts: 22330 Rating: (2999) |
Hi, ok this are many different use cases and problems. 1.) Licencing Yes is it possible to work with TIA Portal V11 and TIA Portal V13 on the same PC with only then TIA V13 licence, no extra TIA V11 licence is needed. And you can install only TIA V11 and transfer the V13 licence to this PC and work with it. 2.)PLC already loaded with V11 To Work with TIA V13 on a already loaded PLC without the old project is possible FAQ for this UseCaseand general FAQ for Uploading 3.) "Can't get into the PLC" What meaning exactly? Can't open the device view of the PLC in TIA or can't go online to the PLC or can't open the blocks of the PLC? Regards Christoph |
Last edited by: ChristophD at: 12/9/2014 12:45 PM |
|
12/9/2014 12:54 PM | |
Posts: 5 Rating: (0) |
I think it might be that we need to open it in compatibiliity mode, I will try it now from the link you provided and see if it works. |
Follow us on