5/6/2016 11:35 AM | |
Joined: 8/25/2006 Last visit: 5/21/2024 Posts: 2205 Rating: (278)
|
Hello. Check in the System parameters of a TCP/IP driver that checkbox Cycle management by PLC is unselected (screen1). If you have selected in Logical Device name TCP/IP(Auto) (like in screen2) then try to switch to TCP/IP -> Broadcom. Attachmentscreen.zip (317 Downloads) |
5/6/2016 12:12 PM | |
Posts: 4 Rating: (0) |
Hello. Cycle management by TDC has been already switched off (unselected). Thanks. |
5/6/2016 12:36 PM | |
Joined: 8/25/2006 Last visit: 5/21/2024 Posts: 2205 Rating: (278)
|
Could you check connection to another PLC's (e.g. S7) via Broadcom-card? |
5/6/2016 3:12 PM | |
Joined: 8/25/2006 Last visit: 5/21/2024 Posts: 2205 Rating: (278)
|
Which FW version have your module CP51M1? What D7-SYS version do you use? |
5/10/2016 8:16 AM | |
Posts: 4 Rating: (0) |
CP51M1 - V 1.1.4 D7-SYS - V 8.0 |
7/11/2016 1:41 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by AutoGen_958870 is split to a separate thread with the subject Communicate between TDC CPU 551 and WinCC 7.3. Best regards |
Follow us on