12/18/2020 10:06 AM | |
Joined: 8/1/2019 Last visit: 5/17/2024 Posts: 299 Rating: (3) |
What exactly does multicast proxy in simatic shell do? |
12/21/2020 7:40 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2146) |
Hello ashadako, the Multicast-Proxy forwards Multicast-Telegrams in see mamual "SIMATIC HMI WinCC V7.5 SP1 WinCC Information System" 5.In the "Multicast Proxy” input field, enter the IP address for the computer intended as "Agent" for the subnet. To add the computer to the list of agents, click "Add". https://support.industry.siemens.com/cs/ww/en/view/109772961/125855967499 and "Information on network technology and UPS" Using routers WinCC V7 can also be used to connect WinCC clients to WinCC servers via routers. WinCC clients without their own project cannot be used for configuration with the routers, only for WinCC Runtime. There are no restrictions for WinCC clients with their own project. The following is required when using routers: https://support.industry.siemens.com/cs/ww/en/view/109772961/102778545419
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to3 thankful Users |
Follow us on