11/26/2012 10:40 PM | |
Joined: 9/27/2006 Last visit: 10/10/2024 Posts: 12286 Rating: (2685) |
Hello Urantia; 1. Here is a webpage from Siemens Energy showing the models of Simeas P available today. http://www.energy.siemens.com/hq/en/automation/power-transmission-distribution/power-quality/power-monitorin-devices/sicam-p.htm?dlsearch=1&fiProductFamily=Power%20Quality%20and%20Measurements&fiProductName=SIMEAS%20P50%20%2F%20P55 I am not sure the P600 isstill available on the market; thereplacement modelfor the P600would be the P55. You can validate in the catalogs available in the Download section (link on that same page). 2. I do not believe there is a Simeas P model designed for Ethernet: they offer Profibus-DP, Modbus-RTU, Modbus-ASCII or IEC 60870-5-103 as integrated protocols. 3. What would you like to do with this new model, read a new circuit and input on the same PLCnetwork? or do you have something different in mind? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/26/2012 10:40 PM |
|
11/27/2012 12:20 AM | |
Joined: 10/23/2009 Last visit: 10/3/2024 Posts: 115 Rating: (0) |
Any suggestions. |
11/27/2012 12:59 AM | |
Joined: 9/27/2006 Last visit: 10/10/2024 Posts: 12286 Rating: (2685) |
Hello Urantia; Your idea of collecting the data using Profibus-DP CPUs would work well, what you have to do is make sure you parametrize the data exchange in order to collect the data you want to collect, See the following manual, Chapters 2 and 3: 7KG7xxx Description Communication Protocol Now, once the PLC has the readings, it would be easy to transfer them by Ethernet to a PC that would archive the data and produce trends as required, WinCC (v. 7.x, for example)would be one option to consider, as it will easily be connected to Siemens PLCs and equipment from other manufacturers, and will archive the recieved data very efficiently.It would also produce alarms on the process, if required. Hope this helps, Daniel Chartier |
7/13/2013 3:13 PM | |
Joined: 3/17/2013 Last visit: 8/25/2024 Posts: 481 Rating: (43) |
Hi |
Follow us on