8/1/2017 6:06 PM | |
Posts: 2 Rating: (0) |
I am looking to communication with the Simcode via Profinet over OPC. Is there an example of this configuration? |
8/1/2017 7:42 PM | |
Joined: 9/27/2006 Last visit: 9/16/2024 Posts: 12282 Rating: (2684) |
Hello wzcredle; Here are 2 links to help you out with OPC UA and Simodcode Pro V. The first is a Siemens presentation on OPC UA on a Simocode Pro V (over Profinet): http://w3.siemens.com/mcms/industrial-controls/en/control-devices-monitoring/motor-management/pages/simocode-pro-with-opc-ua.aspxThe second one is an Application Example, described below: OPC UA - SiemensObjective of the application The objective of the application is to use two practical examples to show you
Main contents of this application This application discusses the following main points:
– on the Comfort Panel and in WinCC V11 – in WinCC Runtime Professional – on the SIMOCODE pro V PN
Hope this helps, Daniel Chartier |
8/4/2017 3:57 PM | |
Posts: 2 Rating: (0) |
Thank you for the information. However I need to use OPC DA, is it possible to do Profinet over OPC DA, possibly using SIMATIC NET software? |
8/4/2017 4:15 PM | |
Joined: 9/27/2006 Last visit: 9/16/2024 Posts: 12282 Rating: (2684) |
Hello wzcredle; Unfortunately every information I can find on Simocode pro communications point to OPC UA only: Simocode pro manages constant-speed, low-voltage motors and provides comprehensive protective, monitoring and control functions. Enjoy the benefits of detailed operating, servicing, and diagnostics data – also for fail-safe disconnection of motors.Communication via PROFIBUS, PROFINET / PROFIsafe, Modbus RTU, and Ethernet IP and OPC UA – which also lets you take advantage of the cloud!See also this presentationSimocode Pro- 2014Hope this helps,Daniel Chartier |
Follow us on