12/24/2023 4:32 PM | |
Joined: 7/15/2009 Last visit: 7/31/2024 Posts: 30 Rating: (0) |
Hello Mr.Ekalavya, what about configuration for this model of Simodrive 611 ,Serial communication RS232C , is it the same PinOut and same configuration with SIMOCOM U Software ? please find attached ,, and please also how can jogging or run the motor with referance speed from SIMOCOM U software,
------------------------------------------------------------------------------------------ AttachmentX411.pdf (293 Downloads) |
Last edited by: Jen_Moderator at: 12/25/2023 12:27:03New subject after splitting |
|
12/26/2023 3:53 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello, Yours is 611 analog drive control card & not 611U or 611D drive. Please refer below manual which will help you to understand RS232 communication. SIMODRIVE 611 analog, Transistor PWM Inverters for AC Feed Drives and AC Main Spindle Drives Hope this helps. |
This contribution was helpful to1 thankful Users |
12/26/2023 4:35 AM | |
Joined: 10/17/2007 Last visit: 9/17/2024 Posts: 4031 Rating: (354)
|
From you picture --you should know--your control card IS NOT 611U but 611A spindle control. SIMOCOM U SW is ONLY FOR 611U, it cannot be used for 611A 611A Spindle control really used a PC software in 1990 (30 years ago) --see attached manual attention that sw is based on MS DOS
AttachmentIBS_manual.pdf (316 Downloads) |
If you like my comments please |
|
This contribution was helpful to1 thankful Users |
12/27/2023 12:34 AM | |
Joined: 7/15/2009 Last visit: 7/31/2024 Posts: 30 Rating: (0) |
Dear Expert ( Mr. nulizhang ), good day to you, thank you very much, i appreciate your very useful information about the different between Simodrive modules 611U & 611A, and also the important information about this old software compatible with 611A with same look like Simatic S5 under dos, anyway i will search for it and try to communicate with the drive module to upload drive parameter, ( by the way, i am sorry i was made a new topic about my problem before see your reply , so please find my attached problem report again to support me. best regards Samir Taha aboSama.
Attachmentproblem report.pdf (272 Downloads) |
12/27/2023 12:59 AM | |
Joined: 7/15/2009 Last visit: 7/31/2024 Posts: 30 Rating: (0) |
Dear Expert, thank you very much , i got this manual and try many to jog the motor manually without any result, the motor only make vibration, also please if you have any information about the motor how to check, i just check the coil ohm about 0.8 ohm between motor phases, the motor name plate doesn't have information about motor volt.
|
Follow us on