Industry Online Support
Technical Forum
11/20/2010 10:54 AM | |
Posts: 2964 Rating: (482) |
Hello..... What type of control is this? what type control card are you using looks like 611U /611A? detail of the connections of the module are attached. you can also refer the same in 611A startup guide. you can see the power module section in SimocomU on the main screen itself Check it out..... Regards, Ekalavya Attachmentmain subject_11.pdf (211 Downloads) |
6/24/2011 3:05 PM | |
Posts: 1 Rating: (0) |
Hello Ekalavya, |
Follow us on