4/20/2016 1:44 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Hello, It is not simodrive 611U but it is 611A i.e. analog drives. Control card 6SN1118-0AA11-0AA1. Please check this once again. Part number says it is closed loop user friendly interface 1 axis FD control card. Where as motor power module is for dual motor. How 2nd motor is interfaced & controlled? However, please refer attached folders, contains termination details of 16/21 Kw infeed regenerative regulated power module & 611A 1 axis control card. HTH. AttachmentAnalog drive control card termination .zip (240 Downloads) |
4/20/2016 2:20 PM | |
Joined: 5/28/2008 Last visit: 6/10/2024 Posts: 4509 Rating: (837) |
Dear Ahmed, Please have a look here in section 4 of this manual. You will found the pins and its designation for controller Card of the SIMODRIVE |
Ayman Elotaify |
|
4/20/2016 2:34 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Dear Sir, Attached manual section 4 is of 611D drive. Part number submitted by Mr. Ahmed is of 611A. There is difference between 611A & 611D drive termination. FYI please. |