2/13/2013 4:16 PM | |
Posts: 8 Rating: (0) |
I checked parameter P-006 (DC link voltage) on the spindle drive and it was close to 600V. Is this parameter meaningful? |
2/13/2013 4:56 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, If you see P-006, it means your drive must be 6SN112X & not 6SC6113. Please confirm. Moreover please check the terminal details. T63 must be there which is not getting enabled. Please see the attached sheet & check the status of T63 in P011. Hope this helps. Attachment611 A P011 Status display.pdf (429 Downloads) |
2/13/2013 5:33 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Please refer the attachment. Attachment611 A P100 status display.pdf (444 Downloads) |
2/15/2013 6:22 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Please refer attached sheet & confirm the LED display is OK. Once if the LED display is confirmed, itwill be confirmed that INFEED module is ok. For the spindle module, can you attach the photograph of spindle drive module or screen shot? This will make easy to dignosis the problem especially P-000orP-100 & P-011. AttachmentInfeed module service display.pdf (388 Downloads) |
Follow us on