Industry Online Support
Technical Forum
1/10/2012 1:53 PM | |
Joined: 8/25/2006 Last visit: 5/3/2024 Posts: 2203 Rating: (277) |
Hello. What value have you set in P102? |
1/10/2012 3:54 PM | |
Posts: 37 Rating: (0) |
23,2A |
1/10/2012 4:39 PM | |
Joined: 8/25/2006 Last visit: 5/3/2024 Posts: 2203 Rating: (277) |
And you really measure about 8A? |
1/10/2012 9:27 PM | |
Posts: 37 Rating: (0) |
Yes. To be sure I measured the field current of the preview mill stand and I found 19A, so it was beginning to weak the field. So the amperemeter was right. |
3/16/2012 4:18 PM | |
Posts: 44 Rating: (6) |
Check also parameters r073.1, r073.2 and p078.2 After change of boards run p051=22 first! regards frimos |
Follow us on