9/27/2022 3:23 AM | |
Joined: 1/17/2013 Last visit: 6/22/2024 Posts: 1090 Rating: (6) |
Dear ChristophD, Can I use SIMOSIM and PLCSim to simulate io-device ? |
Best Regards, |
|
9/27/2022 8:27 AM | |
Joined: 5/12/2006 Last visit: 6/25/2024 Posts: 22276 Rating: (2995)
|
no is not possible |
9/30/2022 6:20 AM | |
Joined: 1/17/2013 Last visit: 6/22/2024 Posts: 1090 Rating: (6) |
Dear ChristophD, At the SIOMTION is it necessary to has real Input/Output to use IO-Device ? |
Best Regards, |
|
9/30/2022 6:26 AM | |
Joined: 5/12/2006 Last visit: 6/25/2024 Posts: 22276 Rating: (2995)
|
no is not need io-devices have is own Transferareas (Input/Output) which is used for transfer |
9/30/2022 8:16 AM | |
Joined: 1/17/2013 Last visit: 6/22/2024 Posts: 1090 Rating: (6) |
Dear ChristophD, I try to do with real SIMOTION and S7-1200 but it not work. How can I do ? |
Best Regards, |
|
Follow us on