2/27/2018 5:39 AM | |
Joined: 2/9/2012 Last visit: 3/15/2024 Posts: 14 Rating: (0) |
Dear experts, We have problem with our simotion D445-2 PN/DP order number 6AU1445-2AD00-0AA0 installed on our rotogravure machine......all leds are blinking in red (please see the attached video) Please suggest us what to do. Thanks in advance. Aris dwi wibowo AttachmentVID 00065-20180227-0853.mov (577 Downloads) |
2/27/2018 6:21 AM | |
Joined: 5/12/2006 Last visit: 8/30/2024 Posts: 22348 Rating: (3006)
|
Hello, this is a System Error (Assert) in the Firmware of the SImotion. Remove CF Card, rename/Delete the User folder, insert card an power on. Go onnline and open diagnostic Buffer of the SIMOTION, save the diagnostic buffer and open a Support request and attach the diagnostic. Regards Christoph |
This contribution was helpful to1 thankful Users |
2/27/2018 7:57 AM | |
Joined: 5/12/2006 Last visit: 8/30/2024 Posts: 22348 Rating: (3006)
|
Hello, yes the CF Card of Simotion can be used with normal CF Card readers.
Christoph |
2/27/2018 3:01 PM | |
Joined: 5/12/2006 Last visit: 8/30/2024 Posts: 22348 Rating: (3006)
|
Hi, is there some card in the Option slot -> remove it. Regards Christoph |
2/28/2018 1:51 AM | |
Joined: 2/9/2012 Last visit: 3/15/2024 Posts: 14 Rating: (0) |
Dear Christoph, There is no option slot installed on the simotion. Regards Aris Dwi wibowo |
3/2/2018 1:34 AM | |
Joined: 2/9/2012 Last visit: 3/15/2024 Posts: 14 Rating: (0) |
Dear experts, Is there anymore solution for this problem...... Thanks Regards, Aris dwi wibowo |
Follow us on