Industry Online Support
Technical Forum
1/8/2009 3:26 PM | |
Joined: 5/12/2006 Last visit: 7/15/2024 Posts: 22312 Rating: (2998)
|
Hello, D435 can be configured as DP Slave. Open the properties tab of the DP- Interface which schould worked as DP-Slave. Select the tab "Operation Mode" and set the checkbox at DP Slave. Further informations you can read in the Communication System Manual of Simotion http://support.automation.siemens.com/WW/view/en/27002464 Regards Christoph |
Follow us on