6/5/2020 6:20 AM | |
Joined: 5/26/2011 Last visit: 8/5/2024 Posts: 456 Rating:
|
Good day experts! Very good thing about SIWAREX is there's a free downloadable project with codes for the FB45 and complete HMI screens for parameterization: https://support.industry.siemens.com/cs/document/28391777 I tried to simulate the program and HMI, so far the parameter values are responding (HMI values transfered to Scale DB9), for instance the DR3 parameters. My question is, how can I simulate the main scale weight value itself? I tried to simulate values on the SIWAREX Hardware Address. It has 8 WORDS, and I found out the 2nd and 3rd WORD corresponds to CH1 Gross Weight and CH1 Digit Value. But even I put some values (which is reflected on the FB45), the HMI scale value is still 0. I also tried to press "calib zero point" and "calib defined weight" still 0. Do I also need to simulate values on the other part of the 8 WORDS hardware address? Thanks. |
Last edited by: G_R_E_Y at: 06/05/2020 07:58:06 |
|
Follow us on