4/29/2016 10:30 PM | |
Posts: 3 Rating: (0) |
Hi .. How can I simulate my program (STEP 7) with a WinCC Flexible 2008 ?? My program is upload to the PLCSIM and I open the WinCC flexible run the interface and there isn´t a result. It´s not comunicating . i'm working with scada system and not HMI and i'm using profibus communication . How can I simulate my program with a winCC flexible together ?? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 5/2/2016 8:51:57 AMNew subject after splitting |
|
5/2/2016 11:01 PM | |
Posts: 3 Rating: (0) |
hello Murof , I am using PLCSIM (PROFIBUS) connection in S7 simulator and In the PGPCSettings I set the PLCSIM DP but I can't solve the problem , it is still not communicating this is screenshot for my project (doc1 (attachement)) please help me if you have any idea ?? AttachmentDoc1.pdf (382 Downloads) |
This contribution was helpful to1 thankful Users |
5/3/2016 2:13 PM | |
Joined: 8/3/2009 Last visit: 9/13/2024 Posts: 13678 Rating: (1726)
|
Hi omayma yes now everything is clear. we can see that you have the Access Point "Softbus". So you have activated the use of S7RTM in PC or HMI Station. So please use the following FAQ without !!Component Configurator!! to get the Accesspoint S7 Online. With Softbus you cannot use the Simulation in HMI Runtime. (you do not need it!!!! you can use the CP5711 without Simatic Net PC Station configuration !!!) https://support.industry.siemens.com/cs/ww/en/view/24109937
Bye Murof |
Last edited by: Murof at: 5/3/2016 2:15:13 PMLast edited by: The Helping Hand at: 5/3/2016 3:00:32 PMMade the link clickable. Last edited by: Murof at: 5/4/2016 8:08:17 AMIf this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |
Follow us on