2/12/2018 4:52 PM | |
Joined: 6/4/2010 Last visit: 6/11/2024 Posts: 380 Rating:
|
Dear Fons, The Desigo XWP controller simulation works together with Desigo CC as well. Please find attached to this post a short guideline about how to do the settings required. The controller simulation can be used for the verification of your Desigo CC graphic engineering with online values from the simulated controller. The Automation Station simulation also helps to increase the engineering efficiency and quality of the PX application. Please note that there is a Desigo CC demo which has its own simulation of the subsystem. Best regards, Albis AttachmentXWPControllerSimulation_DesigoCC_Connection_en.pdf (1049 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on