6/20/2024 9:30 AM | |
Joined: 1/21/2013 Last visit: 7/9/2024 Posts: 2964 Rating:
|
Hi SiforumUser, This is a very specific question and I am not sure if WinCC Unified is the reason for the failure. However, I would like to point out that I am not familiar with SIMOTION or SIMOSIM. I have read that SIMOSIM requires PLCSIM Advanced V3.0 Update 2 or higher. PLCSIM Advanced is able to simulate OPC UA communication when using the 'PLCSIM Virtual Ethernet Adapter' interface. So if you know an option from SIMOSIM to select the adapter for simulation, please make sure that the correct adapter is used. Instead of doing some more tests with WinCC Unified I would recommend to use another tool to test OPC UA. A free OPC UA client that is mentioned in some examples on the Siemens support site is UaExpert®. I have been very satisfied with this tool so far. Kind regards |
Follow us on